JointDriverCollection Class¶
-
class
NXOpen.Motion.
JointDriverCollection
¶ Bases:
object
Represents a collection of Driver objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateJointDriverBuilder | Creates a NXOpen.Motion.JointDriverBuilder |
FindObject | Finds the NXOpen.Motion.JointDriver with the given name. |
Method Detail¶
CreateJointDriverBuilder¶
-
JointDriverCollection.
CreateJointDriverBuilder
¶ Creates a
NXOpen.Motion.JointDriverBuilder
Signature
CreateJointDriverBuilder(jointdriver)
Parameters: jointdriver ( NXOpen.Motion.JointDriver
) –NXOpen.Motion.JointDriver
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.JointDriverBuilder
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
JointDriverCollection.
FindObject
¶ Finds the
NXOpen.Motion.JointDriver
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.JointDriver
.Returns: NXOpen.Motion.JointDriver
with this name.Return type: NXOpen.Motion.JointDriver
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)