JointDefineScrewJointDisplCurveType Enumeration¶
NXOpen.Motion.JointDefine.ScrewJointDisplCurveType is an alias for NXOpen.Motion.JointDefineScrewJointDisplCurveType
-
class
NXOpen.Motion.
JointDefineScrewJointDisplCurveType
¶ Bases:
object
Defines the displacement curve type for screw joints
Enum Members
Enum Member Enum Member Description Spline Spline type Profile Profile type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-