ForceValueTypes Enumeration¶
-
class
NXOpen.Motion.
ForceValueTypes
¶ Bases:
object
Defines function value type Enum Members
Enum Member Enum Member Description Constant constant type use constant value define force magnitude Function function type use function define force magnitude Profile profile type use profiles to define force magnitude -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-