FlexBodyCollection Class¶
-
class
NXOpen.Motion.
FlexBodyCollection
¶ Bases:
object
Represents a collection of flexible body objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreateFlexBodyBuilder | Creates a NXOpen.Motion.FlexBodyBuilder |
FindObject | Finds the NXOpen.Motion.FlexBody with the given name. |
Method Detail¶
CreateFlexBodyBuilder¶
-
FlexBodyCollection.
CreateFlexBodyBuilder
¶ Creates a
NXOpen.Motion.FlexBodyBuilder
Signature
CreateFlexBodyBuilder(flexbody)
Parameters: flexbody ( NXOpen.Motion.FlexBody
) –Returns: Return type: NXOpen.Motion.FlexBodyBuilder
New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
FlexBodyCollection.
FindObject
¶ Finds the
NXOpen.Motion.FlexBody
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.FlexBody
.Returns: NXOpen.Motion.FlexBody
with this name.Return type: NXOpen.Motion.FlexBody
New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)