FlexBodyBuilderPositioning Enumeration¶
NXOpen.Motion.FlexBodyBuilder.Positioning is an alias for NXOpen.Motion.FlexBodyBuilderPositioning
-
class
NXOpen.Motion.
FlexBodyBuilderPositioning
¶ Bases:
object
Represents positioning type of flexible body
Enum Members
Enum Member Enum Member Description AbsoluteOrigin Positioning to absolution place ComponentPosition Positioning to the place where the component is in assembly ThreePointMethod Positioning to user defined place using three point method -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-