DamperCollection Class¶
-
class
NXOpen.Motion.
DamperCollection
¶ Bases:
object
Represents a collection of motion damper
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateDamperBuilder | Return NXOpen.Motion.DamperBuilder object |
FindObject | Finds the NXOpen.Motion.Damper with the given name. |
Method Detail¶
CreateDamperBuilder¶
-
DamperCollection.
CreateDamperBuilder
¶ Return
NXOpen.Motion.DamperBuilder
objectSignature
CreateDamperBuilder(damper)
Parameters: damper ( NXOpen.Motion.Damper
) –NXOpen.Motion.Damper
to be edited, if None then create a new oneReturns: DamperBuilder object Return type: NXOpen.Motion.DamperBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
DamperCollection.
FindObject
¶ Finds the
NXOpen.Motion.Damper
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.Motion.Damper
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)