ControlPortCollection Class¶
-
class
NXOpen.Motion.
ControlPortCollection
¶ Bases:
object
Represents a collection of Control Port objects
To obtain an instance of this class, refer to
NXOpen.Motion.ControlInput
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Motion.ControlPort with the given name. |
Method Detail¶
FindObject¶
-
ControlPortCollection.
FindObject
¶ Finds the
NXOpen.Motion.ControlPort
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.ControlPort
.Returns: NXOpen.Motion.ControlPort
with this name.Return type: NXOpen.Motion.ControlPort
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)