ControlOutputCollection Class¶
-
class
NXOpen.Motion.
ControlOutputCollection
¶ Bases:
object
Represents a collection of Control Output objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateControlOutputBuilder | Creates a NXOpen.Motion.ControlOutputBuilder |
FindObject | Finds the NXOpen.Motion.ControlOutput object with the given name. |
Method Detail¶
CreateControlOutputBuilder¶
-
ControlOutputCollection.
CreateControlOutputBuilder
¶ Creates a
NXOpen.Motion.ControlOutputBuilder
Signature
CreateControlOutputBuilder(controlOutput)
Parameters: controlOutput ( NXOpen.Motion.ControlOutput
) –NXOpen.Motion.ControlOutput
to be editedReturns: ControlOutput object Return type: NXOpen.Motion.ControlOutputBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
ControlOutputCollection.
FindObject
¶ Finds the
NXOpen.Motion.ControlOutput
object with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.ControlOutput
.Returns: NXOpen.Motion.ControlOutput
with this name.Return type: NXOpen.Motion.ControlOutput
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)