ControlOutputBuilderVariableType Enumeration¶
NXOpen.Motion.ControlOutputBuilder.VariableType is an alias for NXOpen.Motion.ControlOutputBuilderVariableType
-
class
NXOpen.Motion.
ControlOutputBuilderVariableType
¶ Bases:
object
Output Variable type
Enum Members
Enum Member Enum Member Description Force Output Variable type Force Torque Output Variable type Torque. ActionTorque Output Variable type Action Torque. Valid only in control output has universal joint as input. BaseTorque Output Variable type Base Torque. Valid only in control output has universal joint as input. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-