ControlInputPortBuilderMeasuredComponent Enumeration¶
NXOpen.Motion.ControlInputPortBuilder.MeasuredComponent is an alias for NXOpen.Motion.ControlInputPortBuilderMeasuredComponent
-
class
NXOpen.Motion.
ControlInputPortBuilderMeasuredComponent
¶ Bases:
object
the types of components that can be measured by the control input element for the selected variable.
Enum Members
Enum Member Enum Member Description LinearMagnitude Linear Magnitude X X Y Y Z Z AngularMagnitude Angular Magnitude Rx RX Ry RY Rz RZ -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-