ControlInputCollection Class¶
-
class
NXOpen.Motion.
ControlInputCollection
¶ Bases:
object
Represents a collection of Control Input objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateControlInputBuilder | Creates a NXOpen.Motion.ControlInputBuilder |
FindObject | Finds the NXOpen.Motion.ControlInput with the given name. |
Method Detail¶
CreateControlInputBuilder¶
-
ControlInputCollection.
CreateControlInputBuilder
¶ Creates a
NXOpen.Motion.ControlInputBuilder
Signature
CreateControlInputBuilder(controlinput)
Parameters: controlinput ( NXOpen.Motion.ControlInput
) –Returns: Return type: NXOpen.Motion.ControlInputBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
ControlInputCollection.
FindObject
¶ Finds the
NXOpen.Motion.ControlInput
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.ControlInput
.Returns: NXOpen.Motion.ControlInput
with this name.Return type: NXOpen.Motion.ControlInput
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)