ConfigurationIntegerParameter Class¶
-
class
NXOpen.Motion.
ConfigurationIntegerParameter
¶ Bases:
NXOpen.Motion.ConfigurationParameter
Represents a
Motion.ConfigurationIntegerParameter
.This class contains the port association for the output of a mechatronics element No KF support
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ActualValue | Returns or sets the actual value |
InitialValue | Returns the initial value |
Name | Returns the name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ActualValue¶
-
ConfigurationIntegerParameter.
ActualValue
¶ Returns or sets the actual value
-------------------------------------
Getter Method
Signature
ActualValue
Returns: Return type: int New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
ActualValue
Parameters: actualValue (int) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
ConfigurationIntegerParameter.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.