BeamForceCollection Class¶
-
class
NXOpen.Motion.
BeamForceCollection
¶ Bases:
object
Represents a collection of BeamForces
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateBeamForceBuilder | Creates a Motion.BeamForceBuilder |
FindObject | Finds the NXOpen.Motion.BeamForce with the given name. |
Method Detail¶
CreateBeamForceBuilder¶
-
BeamForceCollection.
CreateBeamForceBuilder
¶ Creates a
Motion.BeamForceBuilder
Signature
CreateBeamForceBuilder(beamForce)
Parameters: beamForce ( NXOpen.Motion.BeamForce
) –NXOpen.Motion.BeamForce
to be edited, if None then create a new oneReturns: BeamForceBuilder object Return type: NXOpen.Motion.BeamForceBuilder
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
BeamForceCollection.
FindObject
¶ Finds the
NXOpen.Motion.BeamForce
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.BeamForce
Returns: NXOpen.Motion.BeamForce
with this nameReturn type: NXOpen.Motion.BeamForce
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)