AnalyticalContactPropertyCollection Class¶
-
class
NXOpen.Motion.
AnalyticalContactPropertyCollection
¶ Bases:
object
Represents a collection of Analytical Contact Property objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateAnalyticalContactPropertyBuilder | Creates a NXOpen.Motion.AnalyticalContactPropertyBuilder |
FindObject | Finds the NXOpen.Motion.AnalyticalContactProperty with the given name. |
Method Detail¶
CreateAnalyticalContactPropertyBuilder¶
-
AnalyticalContactPropertyCollection.
CreateAnalyticalContactPropertyBuilder
¶ Creates a
NXOpen.Motion.AnalyticalContactPropertyBuilder
Signature
CreateAnalyticalContactPropertyBuilder(analyticalContactProperty)
Parameters: analyticalContactProperty ( NXOpen.Motion.AnalyticalContactProperty
) –Returns: Return type: NXOpen.Motion.AnalyticalContactPropertyBuilder
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
AnalyticalContactPropertyCollection.
FindObject
¶ Finds the
NXOpen.Motion.AnalyticalContactProperty
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.AnalyticalContactProperty
.Returns: NXOpen.Motion.AnalyticalContactProperty
with this name.Return type: NXOpen.Motion.AnalyticalContactProperty
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)