AnalyticalContactCollection Class¶
-
class
NXOpen.Motion.
AnalyticalContactCollection
¶ Bases:
object
Represents a collection of Analytical Contact objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateAnalyticalContactBuilder | Creates a NXOpen.Motion.AnalyticalContactBuilder |
FindObject | Finds the NXOpen.Motion.AnalyticalContact object with the given name. |
Method Detail¶
CreateAnalyticalContactBuilder¶
-
AnalyticalContactCollection.
CreateAnalyticalContactBuilder
¶ Creates a
NXOpen.Motion.AnalyticalContactBuilder
Signature
CreateAnalyticalContactBuilder(analyticalContact)
Parameters: analyticalContact ( NXOpen.Motion.AnalyticalContact
) –NXOpen.Motion.AnalyticalContact
to be editedReturns: AnalyticalContact object Return type: NXOpen.Motion.AnalyticalContactBuilder
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
AnalyticalContactCollection.
FindObject
¶ Finds the
NXOpen.Motion.AnalyticalContact
object with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.AnalyticalContact
.Returns: NXOpen.Motion.AnalyticalContact
with this name.Return type: NXOpen.Motion.AnalyticalContact
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)