ModelingViewHighQualityImageFormatType Enumeration¶
NXOpen.ModelingViewHighQualityImage.FormatType is an alias for NXOpen.ModelingViewHighQualityImageFormatType
-
class
NXOpen.
ModelingViewHighQualityImageFormatType
¶ Bases:
object
Describes the output format of the High Quality Image to be generated
Enum Members
Enum Member Enum Member Description RasterImage A normal single raster image QtvrPanorama Quick Time Virtual Reality panoramic movie, which is a set of images from a fixed viewpoint. The viewer can look in all directions. QtvrObjectLow Quick Time Virtual Reality object movie, which is a set of image of an object in different rotations. The viewer can rotate the object to look at it in any orientation. A low number of frames is generated. QtvrObjectHigh Quick Time Virtual Reality object movie , which is a set of image of an object in different rotations. The viewer can rotate the object to look at it in any orientation. A high number of frames is generated. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-