ModelingViewHighQualityImageDisplayTechniqueType Enumeration¶
NXOpen.ModelingViewHighQualityImage.DisplayTechniqueType is an alias for NXOpen.ModelingViewHighQualityImageDisplayTechniqueType
-
class
NXOpen.
ModelingViewHighQualityImageDisplayTechniqueType
¶ Bases:
object
Describes the technique to be used when generating the High Quality Image
Enum Members
Enum Member Enum Member Description RgbPlusNoise The RGB algorithm is augmented with the addition of random noise to the initial RGB values before the dither takes place. FsRgb The pixel conversion process uses the Floyd-Steinberg dither algorithm to distribute the color error across the picture. This is a recommended mode for 8 bit plane display devices. FsRgbPlusNoise The Floyd-Steinberg algorithm is augmented with the addition of random noise to the initial RGB values before the dither takes place. For some images this method avoids artifacts that can occur using the FS RGB method. Monochrome Pixels are converted to black and white and dithered using the Floyd-Steinberg algorithm. This mode is useful on 1 bit display devices. GrayScale Each pixel is converted to a gray level using the NTSC color to gray scale conversion. NearestRgb Conversion is to the nearest RGB value in the color lookup table. OrderedDither A color dither matrix screens pixel colors. This is a trade of color resolution for screen resolution. This method is faster then the Floyd-Steinberg dither methods but tends to introduce a noticeable pattern in the output image. TcPlusNoise Random noise is added to each pixel where the noise is specifically tailored for true color display devices. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-