ContextMenuEntryType Enumeration¶
NXOpen.MenuBar.ContextMenuEntry.Type is an alias for NXOpen.MenuBar.ContextMenuEntryType
-
class
NXOpen.MenuBar.
ContextMenuEntryType
¶ Bases:
object
Specifies the type of the menu entry.
Enum Members
Enum Member Enum Member Description Submenu Has an attached menu structure containing more entries. PushButton Has a command that is run when this entry is activated. ToggleButton Displays an On/Off state. Separator A visual divider between sections of the menu. Label A label often used to divide and provide context to sub-groups of commands. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-