UDPSignalClientBuilder Class¶
-
class
NXOpen.Mechatronics.
UDPSignalClientBuilder
¶ Bases:
NXOpen.Builder
Represents a
Mechatronics.UDPSignalClientBuilder
builder.This class is sub-object of another builder, and cannot be directly instantiated.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
SelectedConfigurationName | Returns or sets the selected configuration name. |
SelectedConfigurationPart | Returns or sets the selected configuration part. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetConnectionInformation | Gets UDP connection information |
GetConnectionNames | Gets UDP connection names |
GetObject | Returns the object currently being edited by this builder. |
SetConnectionInformation | Sets UDP connection information |
SetConnectionNames | Sets UDP connection names |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Structs¶
UDPSignalClientBuilderSignal_Struct Struct | Represents the data type. |
Property Detail¶
SelectedConfigurationName¶
-
UDPSignalClientBuilder.
SelectedConfigurationName
¶ Returns or sets the selected configuration name.
-------------------------------------
Getter Method
Signature
SelectedConfigurationName
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedConfigurationName
Parameters: configurationName (str) – New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SelectedConfigurationPart¶
-
UDPSignalClientBuilder.
SelectedConfigurationPart
¶ Returns or sets the selected configuration part.
-------------------------------------
Getter Method
Signature
SelectedConfigurationPart
Returns: Return type: NXOpen.Part
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedConfigurationPart
Parameters: ownerPart ( NXOpen.Part
) –New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetConnectionInformation¶
-
UDPSignalClientBuilder.
GetConnectionInformation
¶ Gets UDP connection information
Signature
GetConnectionInformation(connectionName, ownerPart)
Parameters: - connectionName (str) –
- ownerPart (
NXOpen.Part
) –
Returns: a tuple
Return type: A tuple consisting of (castMode, remoteIP, remotePort, localIP, localPort, groupIP, rcvBufSize, sendBufSize, updateTime, signals). castMode is a int. remoteIP is a str. remotePort is a int. localIP is a str. localPort is a int. groupIP is a str. rcvBufSize is a int. sendBufSize is a int. updateTime is a float. signals is a list of
NXOpen.Mechatronics.UDPSignalClientBuilderSignal_Struct
. Array of SignalNew in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetConnectionNames¶
-
UDPSignalClientBuilder.
GetConnectionNames
¶ Gets UDP connection names
Signature
GetConnectionNames()
Returns: a tuple Return type: A tuple consisting of (names, ownerParts). names is a list of str. ownerParts is a list of NXOpen.Part
.New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetConnectionInformation¶
-
UDPSignalClientBuilder.
SetConnectionInformation
¶ Sets UDP connection information
Signature
SetConnectionInformation(connectionName, ownerPart, castMode, remoteIP, remotePort, localIP, localPort, groupIP, rcvBufSize, sendBufSize, updateTime, signals)
Parameters: - connectionName (str) –
- ownerPart (
NXOpen.Part
) – - castMode (int) –
- remoteIP (str) –
- remotePort (int) –
- localIP (str) –
- localPort (int) –
- groupIP (str) –
- rcvBufSize (int) –
- sendBufSize (int) –
- updateTime (float) –
- signals (list of
NXOpen.Mechatronics.UDPSignalClientBuilderSignal_Struct
) – Array of Signal
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetConnectionNames¶
-
UDPSignalClientBuilder.
SetConnectionNames
¶ Sets UDP connection names
Signature
SetConnectionNames(ownerParts, names)
Parameters: - ownerParts (list of
NXOpen.Part
) – - names (list of str) –
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
- ownerParts (list of
Validate¶
-
UDPSignalClientBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.