TransportSurfaceCollection Class¶
-
class
NXOpen.Mechatronics.
TransportSurfaceCollection
¶ Bases:
object
Represents a collection of Transport Surface.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateTransportSurfaceBuilder | Creates a NXOpen.Mechatronics.TransportSurfaceBuilder . |
FindObject | Finds the NXOpen.Mechatronics.TransportSurface with the given name. |
Method Detail¶
CreateTransportSurfaceBuilder¶
-
TransportSurfaceCollection.
CreateTransportSurfaceBuilder
¶ Creates a
NXOpen.Mechatronics.TransportSurfaceBuilder
.Signature
CreateTransportSurfaceBuilder(transportSurface)
Parameters: transportSurface ( NXOpen.Mechatronics.TransportSurface
) –NXOpen.Mechatronics.TransportSurface
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.TransportSurfaceBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
TransportSurfaceCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.TransportSurface
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.TransportSurface
.Returns: NXOpen.Mechatronics.TransportSurface
with this name.Return type: NXOpen.Mechatronics.TransportSurface
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)