TransmitterExitCollection Class¶
-
class
NXOpen.Mechatronics.
TransmitterExitCollection
¶ Bases:
object
Represents a collection of Transmitter Exit.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateTransmitterExitBuilder | Creates a NXOpen.Mechatronics.TransmitterExitBuilder . |
FindObject | Finds the NXOpen.Mechatronics.TransmitterExit with the given name. An exception will be thrown if no object can be found with given name. |
Method Detail¶
CreateTransmitterExitBuilder¶
-
TransmitterExitCollection.
CreateTransmitterExitBuilder
¶ Creates a
NXOpen.Mechatronics.TransmitterExitBuilder
.Signature
CreateTransmitterExitBuilder(transmitterExit)
Parameters: transmitterExit ( NXOpen.Mechatronics.TransmitterExit
) –NXOpen.Mechatronics.TransmitterExit
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.TransmitterExitBuilder
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
TransmitterExitCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.TransmitterExit
with the given name. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.TransmitterExit
.Returns: NXOpen.Mechatronics.TransmitterExit
with this name.Return type: NXOpen.Mechatronics.TransmitterExit
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)