TransmitterEntryCollection Class¶
-
class
NXOpen.Mechatronics.
TransmitterEntryCollection
¶ Bases:
object
Represents a collection of Transmitter Entry.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateTransmitterEntryBuilder | Creates a NXOpen.Mechatronics.TransmitterEntryBuilder . |
FindObject | Finds the NXOpen.Mechatronics.TransmitterEntry with the given name. An exception will be thrown if no object can be found with given name. |
Method Detail¶
CreateTransmitterEntryBuilder¶
-
TransmitterEntryCollection.
CreateTransmitterEntryBuilder
¶ Creates a
NXOpen.Mechatronics.TransmitterEntryBuilder
.Signature
CreateTransmitterEntryBuilder(transmitterEntry)
Parameters: transmitterEntry ( NXOpen.Mechatronics.TransmitterEntry
) –NXOpen.Mechatronics.TransmitterEntry
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.TransmitterEntryBuilder
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
TransmitterEntryCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.TransmitterEntry
with the given name. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.TransmitterEntry
.Returns: NXOpen.Mechatronics.TransmitterEntry
with this name.Return type: NXOpen.Mechatronics.TransmitterEntry
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)