TracerCollection Class¶
-
class
NXOpen.Mechatronics.
TracerCollection
¶ Bases:
object
Represents a collection of Tracer.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateTracerBuilder | Creates a NXOpen.Mechatronics.TracerBuilder . |
FindObject | Finds the NXOpen.Mechatronics.Tracer with the given name. |
Method Detail¶
CreateTracerBuilder¶
-
TracerCollection.
CreateTracerBuilder
¶ Creates a
NXOpen.Mechatronics.TracerBuilder
.Signature
CreateTracerBuilder(tracer)
Parameters: tracer ( NXOpen.Mechatronics.Tracer
) –NXOpen.Mechatronics.Tracer
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.TracerBuilder
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
TracerCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.Tracer
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.Tracer
.Returns: NXOpen.Mechatronics.Tracer
with this name.Return type: NXOpen.Mechatronics.Tracer
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)