ThreeJointCouplerCollection Class¶
-
class
NXOpen.Mechatronics.
ThreeJointCouplerCollection
¶ Bases:
object
Represents a collection of ThreeJointCouplers.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateThreeJointCouplerBuilder | Creates a NXOpen.Mechatronics.ThreeJointCouplerBuilder . |
FindObject | Finds the NXOpen.Mechatronics.ThreeJointCoupler with the given name. |
Method Detail¶
CreateThreeJointCouplerBuilder¶
-
ThreeJointCouplerCollection.
CreateThreeJointCouplerBuilder
¶ Creates a
NXOpen.Mechatronics.ThreeJointCouplerBuilder
.Signature
CreateThreeJointCouplerBuilder(threeJointCouplerConstraint)
Parameters: threeJointCouplerConstraint ( NXOpen.Mechatronics.ThreeJointCoupler
) –NXOpen.Mechatronics.ThreeJointCoupler
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ThreeJointCouplerBuilder
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ThreeJointCouplerCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ThreeJointCoupler
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.ThreeJointCoupler
.Returns: NXOpen.Mechatronics.ThreeJointCoupler
with this name.Return type: NXOpen.Mechatronics.ThreeJointCoupler
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)