TagFormCollection Class

class NXOpen.Mechatronics.TagFormCollection

Bases: object

Represents a collection of TagForm.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX10.0.0.

Methods

Method Description
CreateTagFormBuilder Creates a NXOpen.Mechatronics.TagFormBuilder.
FindObject Finds the NXOpen.Mechatronics.TagFormObject with the given name.

Method Detail

CreateTagFormBuilder

TagFormCollection.CreateTagFormBuilder

Creates a NXOpen.Mechatronics.TagFormBuilder.

Signature CreateTagFormBuilder(tagFormObject)

Parameters:tagFormObject (NXOpen.Mechatronics.TagFormObject) – NXOpen.Mechatronics.TagFormObject to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.TagFormBuilder

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

TagFormCollection.FindObject

Finds the NXOpen.Mechatronics.TagFormObject with the given name.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.TagFormObject.
Returns:NXOpen.Mechatronics.TagFormObject with this name.
Return type:NXOpen.Mechatronics.TagFormObject

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)