SymbolTableBuilderSymbol_Struct Struct¶
NXOpen.Mechatronics.SymbolTableBuilder.Symbol is an alias for NXOpen.Mechatronics.SymbolTableBuilderSymbol_Struct
-
class
NXOpen.Mechatronics.
SymbolTableBuilderSymbol_Struct
¶ Bases:
object
Represents Symbol definition structure.
The Symbol name must be unique in the context of Symbol Table. The comment is optional. . Constructor: NXOpen.Mechatronics.SymbolTableBuilder.Symbol()
Fields¶
Field | Description |
---|---|
Name | Symbol Name |
EIOType | IO type |
EDataType | Data type |
Address | Address |
Comment | Comment Text |
Name¶
-
SymbolTableBuilderSymbol_Struct.
Name
¶ Symbol Name
-------------------------------------
Field Value Type:str
EIOType¶
-
SymbolTableBuilderSymbol_Struct.
EIOType
¶ IO type
-------------------------------------
Field Value Type:
NXOpen.Mechatronics.SymbolTableBuilderIOType
EDataType¶
-
SymbolTableBuilderSymbol_Struct.
EDataType
¶ Data type
-------------------------------------
Field Value Type:
NXOpen.Mechatronics.SymbolTableBuilderDataType