SpeedControlCollection Class¶
-
class
NXOpen.Mechatronics.
SpeedControlCollection
¶ Bases:
object
Represents a collection of Speed Constraint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateSpeedControlBuilder | Creates a NXOpen.Mechatronics.SpeedControlBuilder . |
FindObject | Finds the NXOpen.Mechatronics.SpeedControl with the given name. |
Method Detail¶
CreateSpeedControlBuilder¶
-
SpeedControlCollection.
CreateSpeedControlBuilder
¶ Creates a
NXOpen.Mechatronics.SpeedControlBuilder
.Signature
CreateSpeedControlBuilder(speedControl)
Parameters: speedControl ( NXOpen.Mechatronics.SpeedControl
) –NXOpen.Mechatronics.SpeedControl
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.SpeedControlBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
SpeedControlCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.SpeedControl
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.SpeedControl
.Returns: NXOpen.Mechatronics.SpeedControl
with this name.Return type: NXOpen.Mechatronics.SpeedControl
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)