SignalMappingConnectionCollection Class¶
-
class
NXOpen.Mechatronics.
SignalMappingConnectionCollection
¶ Bases:
object
Represents a collection of Signal Connection.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateConnectionBuilder | Creates a NXOpen.Mechatronics.SignalMappingConnectionBuilder |
FindObject | Finds the NXOpen.Mechatronics.SignalMappingConnection with the given name. |
Method Detail¶
CreateConnectionBuilder¶
-
SignalMappingConnectionCollection.
CreateConnectionBuilder
¶ Creates a
NXOpen.Mechatronics.SignalMappingConnectionBuilder
Signature
CreateConnectionBuilder(connection)
Parameters: connection ( NXOpen.Mechatronics.SignalMappingConnection
) –NXOpen.Mechatronics.SignalMappingConnection
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.SignalMappingConnectionBuilder
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
SignalMappingConnectionCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.SignalMappingConnection
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.SignalMappingConnection
.Returns: NXOpen.Mechatronics.SignalMappingConnection
with this name.Return type: NXOpen.Mechatronics.SignalMappingConnection
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)