SignalAdapterCollection Class

class NXOpen.Mechatronics.SignalAdapterCollection

Bases: object

Represents a collection of Signal Adapter.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX8.5.0.

Methods

Method Description
CreateSignalAdapterBuilder Creates a NXOpen.Mechatronics.SignalAdapterBuilder.
FindObject Finds the NXOpen.Mechatronics.SignalAdapter with the given name.

Method Detail

CreateSignalAdapterBuilder

SignalAdapterCollection.CreateSignalAdapterBuilder

Creates a NXOpen.Mechatronics.SignalAdapterBuilder.

Signature CreateSignalAdapterBuilder(object)

Parameters:object (NXOpen.Mechatronics.SignalAdapter) – NXOpen.Mechatronics.SignalAdapter to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.SignalAdapterBuilder

New in version NX8.5.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

SignalAdapterCollection.FindObject

Finds the NXOpen.Mechatronics.SignalAdapter with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.SignalAdapter.
Returns:NXOpen.Mechatronics.SignalAdapter with this name.
Return type:NXOpen.Mechatronics.SignalAdapter

New in version NX8.5.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)