SensorsActuatorsListBuilder Class¶
-
class
NXOpen.Mechatronics.
SensorsActuatorsListBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.SensorsActuatorsListBuilder
.To create a new instance of this class, use
NXOpen.Mechatronics.PhysicsManager.CreateSensorsActuatorsListBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ObjectName | Returns or sets the object name |
SimitFolder | Returns or sets the simit folder name |
SimitTemplate | Returns or sets the simit template name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetParameterData | Gets all parameter data. |
SetParameterData | Sets all parameter data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Structs¶
SensorsActuatorsListBuilderParameterData_Struct Struct |
|
Property Detail¶
ObjectName¶
-
SensorsActuatorsListBuilder.
ObjectName
¶ Returns or sets the object name
-------------------------------------
Getter Method
Signature
ObjectName
Returns: Return type: str New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ObjectName
Parameters: objectName (str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SimitFolder¶
-
SensorsActuatorsListBuilder.
SimitFolder
¶ Returns or sets the simit folder name
-------------------------------------
Getter Method
Signature
SimitFolder
Returns: Return type: str New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
SimitFolder
Parameters: simitTemplate (str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SimitTemplate¶
-
SensorsActuatorsListBuilder.
SimitTemplate
¶ Returns or sets the simit template name
-------------------------------------
Getter Method
Signature
SimitTemplate
Returns: Return type: str New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
SimitTemplate
Parameters: simitTemplate (str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetParameterData¶
-
SensorsActuatorsListBuilder.
GetParameterData
¶ Gets all parameter data.
Signature
GetParameterData()
Returns: Array of Parameter data Return type: list of NXOpen.Mechatronics.SensorsActuatorsListBuilderParameterData_Struct
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetParameterData¶
-
SensorsActuatorsListBuilder.
SetParameterData
¶ Sets all parameter data.
Signature
SetParameterData(parameterData)
Parameters: parameterData (list of NXOpen.Mechatronics.SensorsActuatorsListBuilderParameterData_Struct
) – Array of Parameter dataNew in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
SensorsActuatorsListBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.