RuntimeFormulaCollection Class¶
-
class
NXOpen.Mechatronics.
RuntimeFormulaCollection
¶ Bases:
object
Represents a collection of RuntimeFormula.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateRuntimeFormulaBuilder | Creates a NXOpen.Mechatronics.RuntimeFormulaBuilder . |
CreateRuntimeFormulaParameterBuilder | Creates a NXOpen.Mechatronics.RuntimeFormulaParameterBuilder |
FindObject | Finds the NXOpen.Mechatronics.RuntimeFormula with the given name. |
Method Detail¶
CreateRuntimeFormulaBuilder¶
-
RuntimeFormulaCollection.
CreateRuntimeFormulaBuilder
¶ Creates a
NXOpen.Mechatronics.RuntimeFormulaBuilder
.Signature
CreateRuntimeFormulaBuilder(formula)
Parameters: formula ( NXOpen.Mechatronics.RuntimeFormula
) –NXOpen.Mechatronics.RuntimeFormula
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.RuntimeFormulaBuilder
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CreateRuntimeFormulaParameterBuilder¶
-
RuntimeFormulaCollection.
CreateRuntimeFormulaParameterBuilder
¶ Creates a
NXOpen.Mechatronics.RuntimeFormulaParameterBuilder
Signature
CreateRuntimeFormulaParameterBuilder(obj)
Parameters: obj ( NXOpen.Mechatronics.RuntimeFormulaParameter
) –NXOpen.Mechatronics.RuntimeFormulaParameter
to be edited, if None then create a new oneReturns: NXOpen.Mechatronics.RuntimeFormulaParameterBuilder
to be edited, if None then create a new oneReturn type: NXOpen.Mechatronics.RuntimeFormulaParameterBuilder
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
RuntimeFormulaCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.RuntimeFormula
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.RuntimeFormula
.Returns: NXOpen.Mechatronics.RuntimeFormula
with this name.Return type: NXOpen.Mechatronics.RuntimeFormula
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)