ReadWriteDeviceCollection Class

class NXOpen.Mechatronics.ReadWriteDeviceCollection

Bases: object

Represents a collection of ReadWriteDevice.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX10.0.0.

Method Detail

CreateReadWriteDeviceBuilder

ReadWriteDeviceCollection.CreateReadWriteDeviceBuilder

Creates a NXOpen.Mechatronics.ReadWriteDeviceBuilder.

Signature CreateReadWriteDeviceBuilder(readWriteObject)

Parameters:readWriteObject (NXOpen.Mechatronics.ReadWriteDeviceObject) – NXOpen.Mechatronics.ReadWriteDeviceObject to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.ReadWriteDeviceBuilder

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

ReadWriteDeviceCollection.FindObject

Finds the NXOpen.Mechatronics.ReadWriteDeviceObject with the given name.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.ReadWriteDeviceObject.
Returns:NXOpen.Mechatronics.ReadWriteDeviceObject with this name.
Return type:NXOpen.Mechatronics.ReadWriteDeviceObject

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)