ProxyOverrideObjectBuilderAttrType Enumeration

NXOpen.Mechatronics.ProxyOverrideObjectBuilder.AttrType is an alias for NXOpen.Mechatronics.ProxyOverrideObjectBuilderAttrType

class NXOpen.Mechatronics.ProxyOverrideObjectBuilderAttrType

Bases: object

the parameter attribute option.

Enum Members

Enum Member Enum Member Description
Bool
Int
Double
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.