ProxyOverrideObjectBuilderAttrBoolValue Enumeration

NXOpen.Mechatronics.ProxyOverrideObjectBuilder.AttrBoolValue is an alias for NXOpen.Mechatronics.ProxyOverrideObjectBuilderAttrBoolValue

class NXOpen.Mechatronics.ProxyOverrideObjectBuilderAttrBoolValue

Bases: object

the value for the boolean option

Enum Members

Enum Member Enum Member Description
False
True
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.