ProfinetClientBuilderTagInfo_Struct Struct¶
NXOpen.Mechatronics.ProfinetClientBuilder.TagInfo is an alias for NXOpen.Mechatronics.ProfinetClientBuilderTagInfo_Struct
-
class
NXOpen.Mechatronics.
ProfinetClientBuilderTagInfo_Struct
¶ Bases:
object
Represents Profinet signal definition structure.
. Constructor: NXOpen.Mechatronics.ProfinetClientBuilder.TagInfo()
Fields¶
Field | Description |
---|---|
StrName | Signal Object |
EDataType | Signal Data Type |
EIOType | Signal IO Type |
Address | Adress value |
BDint | A mark for int DataType ,if true means int32 |
StrName¶
-
ProfinetClientBuilderTagInfo_Struct.
StrName
¶ Signal Object
-------------------------------------
Field Value Type:str
EDataType¶
-
ProfinetClientBuilderTagInfo_Struct.
EDataType
¶ Signal Data Type
-------------------------------------
Field Value Type:
NXOpen.Mechatronics.SignalBuilderDataType
EIOType¶
-
ProfinetClientBuilderTagInfo_Struct.
EIOType
¶ Signal IO Type
-------------------------------------
Field Value Type:
NXOpen.Mechatronics.SignalBuilderExternalSignalIOType