PreventCollisionCollection Class¶
-
class
NXOpen.Mechatronics.
PreventCollisionCollection
¶ Bases:
object
Represents a collection of Prevent Collision Constraint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreatePreventCollisionBuilder | Creates a NXOpen.Mechatronics.PreventCollisionBuilder . |
FindObject | Finds the NXOpen.Mechatronics.PreventCollision with the given name. |
Method Detail¶
CreatePreventCollisionBuilder¶
-
PreventCollisionCollection.
CreatePreventCollisionBuilder
¶ Creates a
NXOpen.Mechatronics.PreventCollisionBuilder
.Signature
CreatePreventCollisionBuilder(preventCollision)
Parameters: preventCollision ( NXOpen.Mechatronics.PreventCollision
) –NXOpen.Mechatronics.PreventCollision
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.PreventCollisionBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
PreventCollisionCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.PreventCollision
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.PreventCollision
.Returns: NXOpen.Mechatronics.PreventCollision
with this name.Return type: NXOpen.Mechatronics.PreventCollision
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)