PositionSensorBuilder Class¶
-
class
NXOpen.Mechatronics.
PositionSensorBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.PositionSensor
builder.To create a new instance of this class, use
NXOpen.Mechatronics.PositionSensorCollection.CreatePositionSensorBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AxisJoint | Returns the joint select. This can be a NXOpen.Mechatronics.HingeJoint , NXOpen.Mechatronics.SlidingJoint , NXOpen.Mechatronics.CylindricalJoint , NXOpen.Mechatronics.PointOnCurveJoint and NXOpen.Mechatronics.PositionControl . |
AxisType | Returns or sets the axis type. |
LowerOutputRange | Returns the lower output range used to scale the position data. Its measure type contains constant, voltage, current |
LowerTrimRange | Returns the lower trim range used to trim the position data. |
MeasureType | Returns or sets the measure type. |
Name | Returns or sets the name. |
Tag | Returns the Tag for this object. |
UpperOutputRange | Returns the upper output range used to scale the position data. |
UpperTrimRange | Returns the upper trim range used to trim the position data. |
UseScale | Returns or sets the use scale flag, which is used to control if the position sensor includes scale parameters. |
UseTrim | Returns or sets the use trim flag, which is used to control if the position sensor includes trim parameters. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PositionSensorBuilderAxisJointType Enumeration | the Axis Joint types. |
PositionSensorBuilderOutputMeasureType Enumeration | the Measure types. |
Property Detail¶
AxisJoint¶
-
PositionSensorBuilder.
AxisJoint
¶ Returns the joint select. This can be a
NXOpen.Mechatronics.HingeJoint
,NXOpen.Mechatronics.SlidingJoint
,NXOpen.Mechatronics.CylindricalJoint
,NXOpen.Mechatronics.PointOnCurveJoint
andNXOpen.Mechatronics.PositionControl
.-------------------------------------
Getter Method
Signature
AxisJoint
Returns: Return type: NXOpen.SelectNXObject
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AxisType¶
-
PositionSensorBuilder.
AxisType
¶ Returns or sets the axis type.
-------------------------------------
Getter Method
Signature
AxisType
Returns: Return type: NXOpen.Mechatronics.PositionSensorBuilderAxisJointType
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AxisType
Parameters: axisType ( NXOpen.Mechatronics.PositionSensorBuilderAxisJointType
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LowerOutputRange¶
-
PositionSensorBuilder.
LowerOutputRange
¶ Returns the lower output range used to scale the position data. Its measure type contains constant, voltage, current
-------------------------------------
Getter Method
Signature
LowerOutputRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LowerTrimRange¶
-
PositionSensorBuilder.
LowerTrimRange
¶ Returns the lower trim range used to trim the position data.
-------------------------------------
Getter Method
Signature
LowerTrimRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MeasureType¶
-
PositionSensorBuilder.
MeasureType
¶ Returns or sets the measure type.
-------------------------------------
Getter Method
Signature
MeasureType
Returns: Return type: NXOpen.Mechatronics.PositionSensorBuilderOutputMeasureType
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MeasureType
Parameters: measureType ( NXOpen.Mechatronics.PositionSensorBuilderOutputMeasureType
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperOutputRange¶
-
PositionSensorBuilder.
UpperOutputRange
¶ Returns the upper output range used to scale the position data.
-------------------------------------
Getter Method
Signature
UpperOutputRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperTrimRange¶
-
PositionSensorBuilder.
UpperTrimRange
¶ Returns the upper trim range used to trim the position data.
-------------------------------------
Getter Method
Signature
UpperTrimRange
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UseScale¶
-
PositionSensorBuilder.
UseScale
¶ Returns or sets the use scale flag, which is used to control if the position sensor includes scale parameters.
-------------------------------------
Getter Method
Signature
UseScale
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
UseScale
Parameters: useScale (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UseTrim¶
-
PositionSensorBuilder.
UseTrim
¶ Returns or sets the use trim flag, which is used to control if the position sensor includes trim parameters.
-------------------------------------
Getter Method
Signature
UseTrim
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
UseTrim
Parameters: useTrim (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
PositionSensorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.