PositionControlCollection Class

class NXOpen.Mechatronics.PositionControlCollection

Bases: object

Represents a collection of Position Control.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX7.5.1.

Method Detail

CreatePositionControlBuilder

PositionControlCollection.CreatePositionControlBuilder

Creates a NXOpen.Mechatronics.PositionControlBuilder.

Signature CreatePositionControlBuilder(positionControl)

Parameters:positionControl (NXOpen.Mechatronics.PositionControl) – NXOpen.Mechatronics.PositionControl to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.PositionControlBuilder

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

PositionControlCollection.FindObject

Finds the NXOpen.Mechatronics.PositionControl with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.PositionControl.
Returns:NXOpen.Mechatronics.PositionControl with this name.
Return type:NXOpen.Mechatronics.PositionControl

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)