PointOnCurveJointCollection Class

class NXOpen.Mechatronics.PointOnCurveJointCollection

Bases: object

Represents a collection of PointOnCurve Joint.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX9.0.0.

Method Detail

CreatePointOnCurveJointBuilder

PointOnCurveJointCollection.CreatePointOnCurveJointBuilder

Creates a NXOpen.Mechatronics.PointOnCurveJointBuilder.

Signature CreatePointOnCurveJointBuilder(joint)

Parameters:joint (NXOpen.Mechatronics.PointOnCurveJoint) – NXOpen.Mechatronics.PointOnCurveJoint to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.PointOnCurveJointBuilder

New in version NX9.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

PointOnCurveJointCollection.FindObject

Finds the NXOpen.Mechatronics.PointOnCurveJoint with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.PointOnCurveJoint.
Returns:NXOpen.Mechatronics.PointOnCurveJoint with this name.
Return type:NXOpen.Mechatronics.PointOnCurveJoint

New in version NX9.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)