PlanarJointCollection Class¶
-
class
NXOpen.Mechatronics.
PlanarJointCollection
¶ Bases:
object
Represents a collection of Planar Joint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreatePlanarJointBuilder | Creates a NXOpen.Mechatronics.PlanarJointBuilder . |
FindObject | Finds the NXOpen.Mechatronics.PlanarJoint with the given name. |
Method Detail¶
CreatePlanarJointBuilder¶
-
PlanarJointCollection.
CreatePlanarJointBuilder
¶ Creates a
NXOpen.Mechatronics.PlanarJointBuilder
.Signature
CreatePlanarJointBuilder(cylinJoint)
Parameters: cylinJoint ( NXOpen.Mechatronics.PlanarJoint
) –NXOpen.Mechatronics.PlanarJoint
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.PlanarJointBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
PlanarJointCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.PlanarJoint
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.PlanarJoint
.Returns: NXOpen.Mechatronics.PlanarJoint
with this name.Return type: NXOpen.Mechatronics.PlanarJoint
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)