PathConstraintJointCollection Class

class NXOpen.Mechatronics.PathConstraintJointCollection

Bases: object

Represents a collection of Path Constraint Joint.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX10.0.0.

Method Detail

CreatePathConstraintJointBuilder

PathConstraintJointCollection.CreatePathConstraintJointBuilder

Creates a NXOpen.Mechatronics.PathConstraintJointBuilder.

Signature CreatePathConstraintJointBuilder(slide)

Parameters:slide (NXOpen.Mechatronics.PathConstraintJoint) – NXOpen.Mechatronics.PathConstraintJoint to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.PathConstraintJointBuilder

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

PathConstraintJointCollection.FindObject

Finds the NXOpen.Mechatronics.PathConstraintJoint with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.PathConstraintJoint.
Returns:NXOpen.Mechatronics.PathConstraintJoint with this name.
Return type:NXOpen.Mechatronics.PathConstraintJoint

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)