ObjectTransformerCollection Class¶
-
class
NXOpen.Mechatronics.
ObjectTransformerCollection
¶ Bases:
object
Represents a collection of Object Transformer.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateObjectTransformerBuilder | Creates a NXOpen.Mechatronics.ObjectTransformerBuilder . |
FindObject | Finds the NXOpen.Mechatronics.ObjectTransformer with the given name. |
Method Detail¶
CreateObjectTransformerBuilder¶
-
ObjectTransformerCollection.
CreateObjectTransformerBuilder
¶ Creates a
NXOpen.Mechatronics.ObjectTransformerBuilder
.Signature
CreateObjectTransformerBuilder(objectSrc)
Parameters: objectSrc ( NXOpen.Mechatronics.ObjectTransformer
) –NXOpen.Mechatronics.ObjectTransformer
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ObjectTransformerBuilder
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ObjectTransformerCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ObjectTransformer
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.ObjectTransformer
.Returns: NXOpen.Mechatronics.ObjectTransformer
with this name.Return type: NXOpen.Mechatronics.ObjectTransformer
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)