ObjectSourceCollection Class

class NXOpen.Mechatronics.ObjectSourceCollection

Bases: object

Represents a collection of Object Source.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX7.5.1.

Methods

Method Description
CreateObjectSourceBuilder Creates a NXOpen.Mechatronics.ObjectSourceBuilder.
FindObject Finds the NXOpen.Mechatronics.ObjectSource with the given name.

Method Detail

CreateObjectSourceBuilder

ObjectSourceCollection.CreateObjectSourceBuilder

Creates a NXOpen.Mechatronics.ObjectSourceBuilder.

Signature CreateObjectSourceBuilder(objectSrc)

Parameters:objectSrc (NXOpen.Mechatronics.ObjectSource) – NXOpen.Mechatronics.ObjectSource to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.ObjectSourceBuilder

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

ObjectSourceCollection.FindObject

Finds the NXOpen.Mechatronics.ObjectSource with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.ObjectSource.
Returns:NXOpen.Mechatronics.ObjectSource with this name.
Return type:NXOpen.Mechatronics.ObjectSource

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)