ObjectSinkCollection Class¶
-
class
NXOpen.Mechatronics.
ObjectSinkCollection
¶ Bases:
object
Represents a collection of Object Sink.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateObjectSinkBuilder | Creates a NXOpen.Mechatronics.ObjectSinkBuilder . |
FindObject | Finds the NXOpen.Mechatronics.ObjectSink with the given name. |
Method Detail¶
CreateObjectSinkBuilder¶
-
ObjectSinkCollection.
CreateObjectSinkBuilder
¶ Creates a
NXOpen.Mechatronics.ObjectSinkBuilder
.Signature
CreateObjectSinkBuilder(objectSrc)
Parameters: objectSrc ( NXOpen.Mechatronics.ObjectSink
) –NXOpen.Mechatronics.ObjectSink
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ObjectSinkBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ObjectSinkCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ObjectSink
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.ObjectSink
.Returns: NXOpen.Mechatronics.ObjectSink
with this name.Return type: NXOpen.Mechatronics.ObjectSink
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)