ObjectInformationBuilder Class¶
-
class
NXOpen.Mechatronics.
ObjectInformationBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ObjectInformationBuilder
This is a sub-builder class and cannot be directly instantiated
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ItemID | Returns or sets the item ID. |
ItemName | Returns or sets the name of item. |
ItemTypes | Returns or sets the item types. |
RevisionID | Returns or sets the revision ID. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDescription | Gets the description. |
GetObject | Returns the object currently being edited by this builder. |
SetDescription | Sets the description. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ItemID¶
-
ObjectInformationBuilder.
ItemID
¶ Returns or sets the item ID.
-------------------------------------
Getter Method
Signature
ItemID
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemID
Parameters: itemID (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ItemName¶
-
ObjectInformationBuilder.
ItemName
¶ Returns or sets the name of item.
-------------------------------------
Getter Method
Signature
ItemName
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemName
Parameters: name (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ItemTypes¶
-
ObjectInformationBuilder.
ItemTypes
¶ Returns or sets the item types.
-------------------------------------
Getter Method
Signature
ItemTypes
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemTypes
Parameters: itemTypes (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RevisionID¶
-
ObjectInformationBuilder.
RevisionID
¶ Returns or sets the revision ID.
-------------------------------------
Getter Method
Signature
RevisionID
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RevisionID
Parameters: revID (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetDescription¶
-
ObjectInformationBuilder.
GetDescription
¶ Gets the description.
Signature
GetDescription()
Returns: Return type: list of str New in version NX8.5.0.
License requirements: None.
SetDescription¶
-
ObjectInformationBuilder.
SetDescription
¶ Sets the description.
Signature
SetDescription(description)
Parameters: description (list of str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ObjectInformationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.