OPCUAClientBuilder Class¶
-
class
NXOpen.Mechatronics.
OPCUAClientBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.OPCUAClientBuilder
builder.This class is sub-object of another builder, and cannot be directly instantiated.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
SelectedConfigurationName | Returns or sets the selected configuration name |
SelectedConfigurationPart | Returns or sets the selected configuration part |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetServerNames | Gets OPC UA instance names |
GetServerTags | Gets OPC UA instance Tags |
SetServerTags | Sets OPC UA instance Tags |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Structs¶
OPCUAClientBuilderTagInfo_Struct Struct |
|
Property Detail¶
SelectedConfigurationName¶
-
OPCUAClientBuilder.
SelectedConfigurationName
¶ Returns or sets the selected configuration name
-------------------------------------
Getter Method
Signature
SelectedConfigurationName
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedConfigurationName
Parameters: configurationName (str) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SelectedConfigurationPart¶
-
OPCUAClientBuilder.
SelectedConfigurationPart
¶ Returns or sets the selected configuration part
-------------------------------------
Getter Method
Signature
SelectedConfigurationPart
Returns: Return type: NXOpen.Part
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedConfigurationPart
Parameters: ownerPart ( NXOpen.Part
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetServerNames¶
-
OPCUAClientBuilder.
GetServerNames
¶ Gets OPC UA instance names
Signature
GetServerNames()
Returns: Return type: list of str New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetServerTags¶
-
OPCUAClientBuilder.
GetServerTags
¶ Gets OPC UA instance Tags
Signature
GetServerTags(serverName)
Parameters: serverName (str) – Returns: Array of TagInfos Return type: list of NXOpen.Mechatronics.OPCUAClientBuilderTagInfo_Struct
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetServerTags¶
-
OPCUAClientBuilder.
SetServerTags
¶ Sets OPC UA instance Tags
Signature
SetServerTags(serverName, tagInfos)
Parameters: - serverName (str) –
- tagInfos (list of
NXOpen.Mechatronics.OPCUAClientBuilderTagInfo_Struct
) – Array of TagInfos
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
OPCUAClientBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.