MotionProfileCollection Class¶
-
class
NXOpen.Mechatronics.
MotionProfileCollection
¶ Bases:
object
Represents a collection of Motion Profile.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateMotionProfileBuilder | Creates a NXOpen.Mechatronics.MotionProfileBuilder . |
FindObject | Finds the NXOpen.Mechatronics.MotionProfile with the given name. |
Method Detail¶
CreateMotionProfileBuilder¶
-
MotionProfileCollection.
CreateMotionProfileBuilder
¶ Creates a
NXOpen.Mechatronics.MotionProfileBuilder
.Signature
CreateMotionProfileBuilder(functionTable)
Parameters: functionTable ( NXOpen.Mechatronics.MotionProfile
) –NXOpen.Mechatronics.MotionProfile
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.MotionProfileBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
MotionProfileCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.MotionProfile
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.MotionProfile
.Returns: NXOpen.Mechatronics.MotionProfile
with this name.Return type: NXOpen.Mechatronics.MotionProfile
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)