MechatronicsSession Class¶
-
class
NXOpen.Mechatronics.
MechatronicsSession
¶ Bases:
object
Represents Mechatronics session
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
GetExportableLogicalObjects | Gets exportable logical objects |
GetLogicalAttributeNames | Gets defined logical attribute names in configuration file |
GetLogicalAttributeValues | Gets attribute values of logical object |
GetLogicalTypes | Gets defined logical types in configuration file |
PerformSimulation | Control the Simulation. |
Enumerations¶
MechatronicsSessionSimulationAction Enumeration | Represents the action of simulation. |
Method Detail¶
GetExportableLogicalObjects¶
-
MechatronicsSession.
GetExportableLogicalObjects
¶ Gets exportable logical objects
Signature
GetExportableLogicalObjects(logicalObject)
Parameters: logicalObject ( NXOpen.Mechatronics.LogicObject
) – Logical objectReturns: Array of exportable logical objects Return type: list of NXOpen.Mechatronics.LogicObject
New in version NX9.0.0.
License requirements: None.
GetLogicalAttributeNames¶
-
MechatronicsSession.
GetLogicalAttributeNames
¶ Gets defined logical attribute names in configuration file
Signature
GetLogicalAttributeNames()
Returns: Array of defined attribute names Return type: list of str New in version NX9.0.0.
License requirements: None.
GetLogicalAttributeValues¶
-
MechatronicsSession.
GetLogicalAttributeValues
¶ Gets attribute values of logical object
Signature
GetLogicalAttributeValues(logicalObject, attributeNames)
Parameters: - logicalObject (
NXOpen.Mechatronics.LogicObject
) – Logical object - attributeNames (list of str) – Array of logical attribute names
Returns: Array of logical attribute values
Return type: list of str
New in version NX9.0.0.
License requirements: None.
- logicalObject (
GetLogicalTypes¶
-
MechatronicsSession.
GetLogicalTypes
¶ Gets defined logical types in configuration file
Signature
GetLogicalTypes()
Returns: a tuple Return type: A tuple consisting of (logicalTypeNames, logicalTypeBitmaps) logicalTypeNames is a list of str. Array of type names logicalTypeBitmaps is a list of str. Array of type bitmaps New in version NX9.0.0.
License requirements: None.
PerformSimulation¶
-
MechatronicsSession.
PerformSimulation
¶ Control the Simulation.
Signature
PerformSimulation(action)
Parameters: action ( NXOpen.Mechatronics.MechatronicsSessionSimulationAction
) –New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)