MATLABSignalConnectionCollection Class¶
-
class
NXOpen.Mechatronics.
MATLABSignalConnectionCollection
¶ Bases:
object
Represents a collection of Signal Connection.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateSignalConnectionBuilder | Creates a NXOpen.Mechatronics.MATLABSignalConnectionBuilder |
FindObject | Finds the NXOpen.Mechatronics.MATLABSignalConnection with the given name. |
Method Detail¶
CreateSignalConnectionBuilder¶
-
MATLABSignalConnectionCollection.
CreateSignalConnectionBuilder
¶ Creates a
NXOpen.Mechatronics.MATLABSignalConnectionBuilder
Signature
CreateSignalConnectionBuilder(connection)
Parameters: connection ( NXOpen.Mechatronics.MATLABSignalConnection
) –NXOpen.Mechatronics.MATLABSignalConnection
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.MATLABSignalConnectionBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
MATLABSignalConnectionCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.MATLABSignalConnection
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.MATLABSignalConnection
.Returns: NXOpen.Mechatronics.MATLABSignalConnection
with this name.Return type: NXOpen.Mechatronics.MATLABSignalConnection
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)