LinearSpringJointCollection Class

class NXOpen.Mechatronics.LinearSpringJointCollection

Bases: object

Represents a collection of Linear Spring Joint.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX7.5.1.

Method Detail

CreateLinearSpringJointBuilder

LinearSpringJointCollection.CreateLinearSpringJointBuilder

Creates a NXOpen.Mechatronics.LinearSpringJointBuilder.

Signature CreateLinearSpringJointBuilder(linearSpringJoint)

Parameters:linearSpringJoint (NXOpen.Mechatronics.LinearSpringJoint) – NXOpen.Mechatronics.LinearSpringJoint to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.LinearSpringJointBuilder

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

LinearSpringJointCollection.FindObject

Finds the NXOpen.Mechatronics.LinearSpringJoint with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.LinearSpringJoint.
Returns:NXOpen.Mechatronics.LinearSpringJoint with this name.
Return type:NXOpen.Mechatronics.LinearSpringJoint

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)